FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Precautions taken when QJ61BT11 is replaced with QJ61BT11N
FAQ
Precautions taken when QJ61BT11 is replaced with QJ61BT11N
Are there any precautions that must be followed when QJ61BT11 is replaced with QJ61BT11N?
- Category :
Answer
Set the Network Parameter as shown below.
(1) If QJ61BT11 is in the remote net mode, use the remote net Ver.1 mode for QJ61BT11N.
(2) If QJ61BT11 is in the remote I/O net mode, use the remote I/O net mode for QJ61BT11N.
For more details, refer to the following manual.
- CC-Link System Master/Local Module User's Manual
Appendix 5 Difference from traditional modules
Appendix 5.2 Precautions when replacing a QJ61BT11 with a QJ61BT11N
(1) If QJ61BT11 is in the remote net mode, use the remote net Ver.1 mode for QJ61BT11N.
(2) If QJ61BT11 is in the remote I/O net mode, use the remote I/O net mode for QJ61BT11N.
For more details, refer to the following manual.
- CC-Link System Master/Local Module User's Manual
Appendix 5 Difference from traditional modules
Appendix 5.2 Precautions when replacing a QJ61BT11 with a QJ61BT11N
- Product Name
- Network Related Products
- Series
- CC-Link