FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Buffer memory addresses of CC-Link modules
FAQ
Buffer memory addresses of CC-Link modules
I want to write and read data using FROM/TO instructions in CC-Link communication. Does each station number have fixed buffer memory addresses for them to be assigned?
- Category :
Answer
If the remote net Ver.1 mode is used, each station number is given fixed buffer memory addresses.
If the remote net Ver.2 mode is used, different buffer memory addresses are given according to the type of slave station and the number of points the slave station takes.
If the remote net Ver.2 mode is used, different buffer memory addresses are given according to the type of slave station and the number of points the slave station takes.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Difference between CC-Link reserved stations and invalid stations
- Parameter settings for a CC-Link master station and local stations
- CC-Link slave station's flashing L.ERR LED
- Difference in specifications between "AJ65SBTB1" and "AJ65SBTB2" in CC-Link remote I/O modules' model names
- Reception data read request signal of QJ71C24N not turn ON