FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > How to set CC-Link reserved stations
FAQ
How to set CC-Link reserved stations
How do I set a CC-Link reserved station?
- Category :
Answer
- If the Network Parameter is used
Make "Station Information Setting".
- If the parameter is set using a dedicated instruction
Set the control data of the RLPASET instruction.
Make "Station Information Setting".
- If the parameter is set using a dedicated instruction
Set the control data of the RLPASET instruction.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- PLC parameter setting for QJ61BT11N
- CC-Link master modules' start I/O No. and refresh devices RX/RY
- About network parameters when building MELSECNET/10 with Q02HCPU-A
- Connecting terminating resistors to the sending end and the receiving end in communication of QJ71C24N
- Difference in specifications between "AJ65SBTB1" and "AJ65SBTB2" in CC-Link remote I/O modules' model names