FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Detecting the number of disconnections when using QJ71E71-100
FAQ
Detecting the number of disconnections when using QJ71E71-100
Are there any methods of detecting the number of disconnections when QJ71E71-100 is used?
- Category :
Answer
The number of disconnections detected can be checked by reading the buffer memory address 5203H (Disconnection detection count). Disconnections are detected when the following events occur.
- QJ71E71-100 is disconnected from the hub.
- A cable is removed from a hub connector.
- The hub is powered OFF.
- QJ71E71-100 Version D or later supports the capability of counting the disconnections due to cable removal from
the QJ71E71-100 connector.
- QJ71E71-100 is disconnected from the hub.
- A cable is removed from a hub connector.
- The hub is powered OFF.
- QJ71E71-100 Version D or later supports the capability of counting the disconnections due to cable removal from
the QJ71E71-100 connector.
- Product Name
- Network Related Products
- Series
- Ethernet Interface Module
May I have your opinion?
Related FAQ
- Executing the QJ71C24N's pre-defined protocol support function
- SLD and FG wiring for CC-Link networks
- Connecting terminating resistors to the sending end and the receiving end in communication of QJ71C24N
- CC-Link slave station's flashing L.ERR LED
- Connecting the CC-Link IE Field Network with a personal computer