FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Effect on sequence scans in MELSECNET/H networks
FAQ
Effect on sequence scans in MELSECNET/H networks
When the refresh parameter for a MELSECNET/H network is set, the sequence scan time becomes longer.How do I reduce the scan time?
- Category :
Answer
It is necessary to reduce the link refresh time of the MELSECNET/H network in order to reduce the scan time.
The link refresh time can be reduced by reducing the number of refresh points assigned to the CPU module. Reduce the refresh points using either of the following methods:
(1) Using the refresh parameter
Set the refresh parameter so that only necessary areas are refreshed.
(2) Direct access to link devices
The refresh time can be reduced by directly accessing link devices used less frequently by the host station and excluding
them from the refresh range.
The link refresh time can be reduced by reducing the number of refresh points assigned to the CPU module. Reduce the refresh points using either of the following methods:
(1) Using the refresh parameter
Set the refresh parameter so that only necessary areas are refreshed.
(2) Direct access to link devices
The refresh time can be reduced by directly accessing link devices used less frequently by the host station and excluding
them from the refresh range.
- Product Name
- Network Related Products
- Series
- MELSECNET/H