FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Communication between CPU modules established by QJ71E71
FAQ
Communication between CPU modules established by QJ71E71
What mode of communication between CPU modules is provided by the QJ71E71 series modules?
- Category :
Answer
The communication between QJ71E71 series modules can be established if READ/WRITE instructions are used.
- Product Name
- Network Related Products
- Series
- Ethernet Interface Module
May I have your opinion?
Related FAQ
- Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function
- Receiving data when no receive complete code is designated (QJ71C24N)
- Connecting QJ71C24N to an external device that has no DTR signal
- Limitation on the number of levels of cascade connections when QJ71E71-100 is used
- Difference between AJ65SBTB1-16DT and AJ65SBTB1-16DT1