FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Receiving data when no receive complete code is designated (QJ71C24N)
FAQ
Receiving data when no receive complete code is designated (QJ71C24N)
What methods of receiving data do the QJ71C24N series modules provide if no receive complete code is designated?
- Category :
Answer
Data are received on a received data count basis. If there is no receive complete code and variable length data is received, the data is received at every non reception monitoring time period.
- Product Name
- Network Related Products
- Series
- Computer Link / Serial Communication
May I have your opinion?
Related FAQ
- Connecting QJ71C24N to an external device that has no DTR signal
- Applicable size for plug-in connector socket block on QJ71C24N-R4
- Limitation on the number of levels of cascade connections when QJ71E71-100 is used
- Order in which a CC-Link master module and slave stations are connected
- Difference between AJ65SBTB1-16DT and AJ65SBTB1-16DT1