FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Connecting QJ71C24N to an external device that has no DTR signal
FAQ
Connecting QJ71C24N to an external device that has no DTR signal
How do I connect QJ71C24N(-R2) to an external device that has no DTR signal for RS-232?
- Category :
Answer
Carry out DTR and DSR wiring that returns signals on QJ71C24N(-R2).
- Product Name
- Network Related Products
- Series
- Computer Link / Serial Communication
May I have your opinion?
Related FAQ
- Limitation on the number of levels of cascade connections when QJ71E71-100 is used
- Receiving data when no receive complete code is designated (QJ71C24N)
- Communication between CPU modules established by QJ71E71
- Applicable size for plug-in connector socket block on QJ71C24N-R4
- Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function