Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23309
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

Why can not a auxiliary contact unit be installed in S-T100DL or less?
Category : 

Answer

This is because the delay time becomes shorter since the rebound force ofa spring against the suction force of a magnetic contactor increases if thecontact "a" is added to a auxiliary contact, although structually it ispossible to install a auxiliary contact unit. It is supposed to meet the delaytime of 1 to 4 seconds, but the delay time can not be guaranteed due tothe addition of a auxiliary contact.
Product Name
Motor Starters
Series
MS-T/N
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?