Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23346
  • Release Date : 2018/09/12 15:12
  • Print

About Low-voltage Power Distribution Products

If ambient temperature of a solid state contactor is more than 60℃,is it possible to use it? If not, how can I deal with?
Category : 

Answer

The maximum ambient temparature for US-N/K/H type is 60℃ and theycan not be used with more than 60℃. If the temparature is more than60℃, you need to consider cooling inside of control panel by clearing theair with cooling fan etc. (Moreover, you need to reduce the current whenthe ambient temparature is more than 40℃.)
Product Name
Motor Starters
Series
MS-T/N

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries