FAQ


FAQAbout Products
 - FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
 
FAQ
About Low-voltage Power Distribution Products
      If ambient temperature of a solid state contactor is more than 60℃,is it possible to use it? If not, how can I deal with?
    
  
Answer
    The maximum ambient temparature for US-N/K/H type is 60℃ and theycan not be used with more than 60℃. If the temparature is more than60℃, you need to consider cooling inside of control panel by clearing theair with cooling fan etc. (Moreover, you need to reduce the current whenthe ambient temparature is more than 40℃.)
  
    - Product Name
 - Motor Starters
 
- Series
 - MS-T/N