Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23603
  • Release Date : 2018/09/14 15:09
  • Print

Parameter initialization

Answer

The following shows the initialization procedure.
(1) Turn OFF the PLC ready flag.
(2) Turn ON "[Cd.2] Parameter initialization request".
    Set "1" to the buffer memory 1901. After the completion of initialization, "0" is automatically set to the buffer memory 1901.
(3) Reset the PLC CPU, or turn the power OFF to ON.
Product Name
Simple Motion module
Series
MELSEC iQ-R
MELSEC iQ-F
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?