FAQ
FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Simple Motion Modules > RD77GF > Parameter initialization
FAQ
Parameter initialization
How do I initialize the parameters?
- Category :
Answer
The following shows the initialization procedure.
(1) Turn OFF the PLC ready flag.
(2) Turn ON "[Cd.2] Parameter initialization request".
Set "1" to the buffer memory 1901. After the completion of initialization, "0" is automatically set to the buffer memory 1901.
(3) Reset the PLC CPU, or turn the power OFF to ON.
(1) Turn OFF the PLC ready flag.
(2) Turn ON "[Cd.2] Parameter initialization request".
Set "1" to the buffer memory 1901. After the completion of initialization, "0" is automatically set to the buffer memory 1901.
(3) Reset the PLC CPU, or turn the power OFF to ON.
- Product Name
- Simple Motion module
- Series
- MELSEC iQ-R
MELSEC iQ-F