Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23621
  • Release Date : 2018/09/14 15:09
  • Print

Torque limit

How can I stop the operation when the motor is stuck in something, resulting in increased torque?
Category : 

Answer

Torque is limited by the lower set value of "[Pr.17] Torque limit setting value" and "[Cd.22] New torque value/forward new torque value".
When the current torque reaches the limit, "b13: Torque limit" of "[Md.108] Servo status1" turns ON.
Create a program so that this flag is used as a trigger of an operation stop or an operation start in reverse direction.
But when using such programs, note that the torque limit flag could also be turned ON when torque increases at a rapid acceleration.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?