FAQ
FAQAbout Products
- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J3 > Difference between the current command and torque
FAQ
Difference between the current command and torque
There are “current command” and “torque” in the monitor value (graph function such in the analog monitor and MR Configurator2, etc.). What is the difference between them?
- Category :
Answer
The “current command” is the command value for the current control (torque control) and the “torque” is the feedback value controlled by the current control (torque control).
The servo motor generates the torque according to the current flowing from the servo amplifier, and “current command” and “torque” will be in a relationship of command and feedback.
The servo motor generates the torque according to the current flowing from the servo amplifier, and “current command” and “torque” will be in a relationship of command and feedback.
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MELSERVO Others