FAQ


FAQAbout Products
- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J4 > Changing multiplication of analog torque command
FAQ
Changing multiplication of analog torque command
Use the analog torque command to control the torque.
I want to set to output the maximum torque when I input 5 V.
Is it possible?
I want to set to output the maximum torque when I input 5 V.
Is it possible?
- Category :
Answer
Yes, it is.
For MR-J4-A/MR-J3-A,
set by [Pr. PC13].
As the initial value (100.0%), the maximum torque is generated at ±8 V.
To generate the maximum torque at ±5 V,
change the setting to [Pr. PC13] = 160.0 (= 8 V/5 V*100.0)
.
The parameter number, etc. may differ depending on the model.
For details, refer to each servo amplifier instruction manual.
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO Others