FAQ


FAQAbout Products
 - FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J4 > Changing multiplication of analog torque command
 
FAQ
Changing multiplication of analog torque command
      Use the analog torque command to control the torque. 
I want to set to output the maximum torque when I input 5 V.
Is it possible?
  I want to set to output the maximum torque when I input 5 V.
Is it possible?
- Category :
 
Answer
Yes, it is.
For MR-J4-A/MR-J3-A, 
set by [Pr. PC13]. 
As the initial value (100.0%), the maximum torque is generated at ±8 V. 
To generate the maximum torque at ±5 V, 
change the setting to [Pr. PC13] = 160.0 (= 8 V/5 V*100.0)
. 
The parameter number, etc. may differ depending on the model. 
For details, refer to each servo amplifier instruction manual. 
- Product Name
 - AC Servos-MELSERVO
 
- Series
 - MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO Others