FAQ


FAQAbout Products
- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J4 > Servo motor does not rotate when the command pulse is input.
FAQ
Servo motor does not rotate when the command pulse is input.
Servo motor does not rotate when the command pulse is input from the positioning module.
- Category :
Answer
The pulse train form outputted with the controller and the setting of servo amplifier (command pulse input form) may differ.
Check the parameter settings. (MR-J4-A: [Pr.PA13])
For the other causes, refer to “No Motor Rotation”, etc. of MR Configurator2 (servo setup software) to investigate. (* Some models are not supported.)
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MELSERVO Others