Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23635
  • Release Date : 2018/09/14 15:10
  • Print

Specifying the axis in test operation of MR-J4W

I want to run a test operation to the B axis of MR-J4W2-B. However, only axis 1 is displayed. How can I select the other axes?
Category : 

Answer

When the MR-J4-B is selected on the model selection screen at creating a new project, the multi-axis check box will be enabled. Click the check box and select the axis to test from A, B or C (MR-J4W3-B only).
The test operation is performed to this axis. (A axis = axis 1, B axis = axis 2, C axis = axis 3)
When running a test operation to another axis, create a new project.

Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-J3, MR Configurator2
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?