Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23640
  • Release Date : 2018/09/14 15:10
  • Print

Positioning operation

Can I check the positioning operation without using the controller?
Category : 

Answer

Using MR Configurator2, you can perform the positioning operation when there is no command from the controller.
You can perform the operation specifying the travel distance (pulse), motor speed and acceleration/deceleration time constants. Or, you can perform the operation the specified number of times by selecting the repeat pattern (forward/reverse rotation, etc.)
Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MR Configurator2
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?