FAQ


FAQAbout Products

- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J3 > Positioning operation
FAQ
Positioning operation
Can I check the positioning operation without using the controller?
- Category :
Answer
Using MR Configurator2, you can perform the positioning operation when there is no command from the controller.
You can perform the operation specifying the travel distance (pulse), motor speed and acceleration/deceleration time constants. Or, you can perform the operation the specified number of times by selecting the repeat pattern (forward/reverse rotation, etc.)
You can perform the operation specifying the travel distance (pulse), motor speed and acceleration/deceleration time constants. Or, you can perform the operation the specified number of times by selecting the repeat pattern (forward/reverse rotation, etc.)
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MR Configurator2