FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > AC Servos-MELSERVO > Servo Support Software > Motor-less operation
FAQ
Motor-less operation
Can I debug only by the servo amplifier without connecting the servo motor?
- Category :
Answer
The servo amplifier has the motor-less operation function.
Without connecting the servo motor, output signals or status display can be provided in response to the input device as if the servo motor is actually running. This operation can be used to check the sequence of a controller, etc.
Some models such as linear servo motor are not supported for this operation. Refer to the instruction manual.
Without connecting the servo motor, output signals or status display can be provided in response to the input device as if the servo motor is actually running. This operation can be used to check the sequence of a controller, etc.
Some models such as linear servo motor are not supported for this operation. Refer to the instruction manual.
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MR Configurator2