Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24807
  • Release Date : 2019/03/27 12:12
  • Print

Wire length for analog output and contact output(ME96SS series)

How long is the maximum wire length that can be used for ME96SS contact output or analog output?
Category : 

Answer

It depends on the service conditions.
Refer to the following guidelines.

① Contact output
     Contact output for ME96 series is no-voltage "a" contact.
     The wire length shall be up to 2km.

  

② Analog output
     The resistance value connected to analog output of ME96SS series shall be 600Ω or less.
     The wire length shall be up to 2km.

Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?