FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Communication format setting
FAQ
Communication format setting
How can I set the communication format?
Answer
The communication format can be set in the communication setting of a sequence program or "PLC Parameter setting" using GX Developer.
To avoid setting troubles, use either method.
To avoid setting troubles, use either method.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit, Engineering Software, GX Works2, GX Developer
May I have your opinion?
Related FAQ
- Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
- Overwriting a current value with the high-speed counter comparison instruction
- Comment display
- Maximum number of characters in a comment that can be transferred to a FX3U series
- Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block