- No : 22306
- Release Date : 2018/08/30 13:55
-
Print
Regarding CW/CCW(Forward pulse/Reverse pulse) output of the built-in positioning function
Does CPU built-in positioning function support CW/CCW(Forward pulse/Reverse pulse) output?
- Category :
-
Answer
Yes, CW/CCW outputs are supported.
Up to 2 axes can be controlled by setting parameter from GX Works3.
Also, by adding high speed pulse input/output module, up to 8 axes can be added.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Simple Motion/Positioning Control
- Series
- MELSEC iQ-F Series