FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding CW/CCW(Forward pulse/Reverse pulse) output of the built-in positioning function
FAQ
Regarding CW/CCW(Forward pulse/Reverse pulse) output of the built-in positioning function
Does CPU built-in positioning function support CW/CCW(Forward pulse/Reverse pulse) output?
Answer
FX5U/FX5UC/FX5S CPU modules are supported. Up to 2 axes are available in GX Works3 parameter settings.
In addition, up to 8 axes can be added by adding a high-speed pulse I/O module.
The built-in positioning function of the FX5UJ CPU module does not support CW/CCW output. Up to 8 axes can be added by adding a high-speed pulse I/O module.
In addition, up to 8 axes can be added by adding a high-speed pulse I/O module.
The built-in positioning function of the FX5UJ CPU module does not support CW/CCW output. Up to 8 axes can be added by adding a high-speed pulse I/O module.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Motion/Positioning
- Series
- MELSEC iQ-F Series