- No : 22317
- Release Date : 2018/08/30 13:55
-
Print
Regarding setting CC-Link settings using GX Works3
Is it possible to set the CC-Link settings through the parameter settings of GX Works3?
- Category :
-
Answer
Parameters can be set when connecting the MELSEC iQ-F series with FX5-CCL-MS(CC-Link system master/intelligent device).
However, when connecting with FX3U-16CCL-M(CC-Link master), the settings must be configured using a program.
For further details, please refer to the example programs in FX3U-16CCL-M User's Manual.
12.1.3 Setting of parameters
1. Program for parameters
- Product Name
- FX3U-16CCL-M, FX5-CCL-MS
- Product Category
- CPU Module, Network/Communication, Engineering Software, GX Works3
- Series
- FX5U,FX5UC