FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS > Error 108
FAQ
Error 108
What is error 108?
What should I do when it occurs?
What should I do when it occurs?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77GF
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75M
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD74MH
Answer
Error 108 (Start not possible) occurs when a start is requested while a stop signal is ON.
Check the "[Md.26] Axis operation status".If "20: Servo amplifier has not been connected/servo amplifier power OFF" is set, turn ON the control circuit of the servo amplifier.
Be sure not to request a start when the axis operation state is other
than "0: standby", "1: stopped", and "-2: step standby".
Check the "[Md.26] Axis operation status".If "20: Servo amplifier has not been connected/servo amplifier power OFF" is set, turn ON the control circuit of the servo amplifier.
Be sure not to request a start when the axis operation state is other
than "0: standby", "1: stopped", and "-2: step standby".
- Product Name
- Simple Motion module/
Positioning module
- Series
- MELSEC-Q
MELSEC-L