FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Comparison result of the CMP instruction
FAQ
Comparison result of the CMP instruction
When the CMP instruction is executed, the comparison result is not cleared even after the command input turns off.
- Category :
Answer
A comparison result is held even after the command input turns off. The remaining comparison result can be cleared by using the RST or ZRST instruction.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series
May I have your opinion?
Related FAQ
- Maximum number of characters in a comment that can be transferred to a FX3U series
- Terminal blocks for the MELSEC-F series
- Connecting a USB interface of a personal computer to a programmable controller
- Modules that support differential line driver outputs
- Index modifier of the bit device in the FX3GC series