FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Connecting a USB interface of a personal computer to a programmable controller
FAQ
Connecting a USB interface of a personal computer to a programmable controller
The personal computer, with GX Works2 installed, only has a USB interface.
How can I connect the personal computer to a programmable controller?
How can I connect the personal computer to a programmable controller?
- Category :
Answer
・ The FX-USB-AW can be used for the programmable controllers except for the FX3S/FX3G/FX3GC series.
・ Since the FX3S/FX3G/FX3GC series have the built-in USB port, a personal computer can be connected using a USB cable, GT09-C30USB-5P or MR-3JUSBCBL3M.
To use the FX-USB-AW, install the USB driver provided with the FX-USB-AW, on the personal computer.
For details on how to install the USB driver, refer to the following.
Appendix 16 in the GX Works2 Version 1 Operating Manual (Common) (Manual number: SH-080779ENG)
* The personal computer can also be connected to the FX3U and FX3UC series using the FX3U-USB-BD.
・ Since the FX3S/FX3G/FX3GC series have the built-in USB port, a personal computer can be connected using a USB cable, GT09-C30USB-5P or MR-3JUSBCBL3M.
To use the FX-USB-AW, install the USB driver provided with the FX-USB-AW, on the personal computer.
For details on how to install the USB driver, refer to the following.
Appendix 16 in the GX Works2 Version 1 Operating Manual (Common) (Manual number: SH-080779ENG)
* The personal computer can also be connected to the FX3U and FX3UC series using the FX3U-USB-BD.
- Product Name
- FX-USB-AW, FX3U-USB-BD
- Product Category
- Main unit, Accessories, Options, Engineering Software, GX Works2, GX Developer
- Series
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
May I have your opinion?
Related FAQ
- Built-in variable analog potentiometers of the FX3G series
- External appearance of the F2-40BL
- Communication setting methods when the FX3U-232-BD is used
- Latch (backup) areas in the data register (D) and extended register (R) of the FX3U/FX3UC series
- Externally switching the operating status of a programmable controller