Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24781
  • Release Date : 2019/02/27 16:10
  • Print

Settings for the FX3U-ENET-ADP

Which software and peripherals are required to set parameters for the FX3U-ENET-ADP (for Ethernet communications)?
Category : 

Answer

GX Works2 with Ver. 1.87R or later is required. 
Product Name
FX3U-ENET-ADP
Product Category
Network/Communication, Engineering Software, GX Works2, GX Developer
Series
FX3S, FX3G, FX3GC, FX3U, FX3UC
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?