FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Input filter adjustment when a high-speed counter or the interrupt function is used
FAQ
Input filter adjustment when a high-speed counter or the interrupt function is used
Is it necessary to adjust the input filter when a high-speed counter or the interrupt function is used?
Answer
When a coil of the high-speed counter or an interrupt pointer is programmed, the programmable controller system adjusts the filter constant of the corresponding input terminal to a minimum value automatically.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- High-Speed Counter
- Series
- MELSEC-F Series
May I have your opinion?
Related FAQ
- Regarding changing the current value of the high-speed counter.
- Regarding the Certificate of non-applicability to export to other countries
- Regarding model name of CC-Link cables
- Regarding the number of available channels of the built-in high speeed counters.
- Regarding the frequency of high-speed counters