Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
>
Index modifier of bit devices in the ...
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
No : 24959
Release Date : 2019/04/18 14:35
Print
Index modifier of bit devices in the FX3G series
Is it possible to use the index modifier for the bit devices, such as LD X0Z0 OUT Y0, in the FX3G series?
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
The FX3G series does not support the index modifier for the bit devices. The FX3U/FX3UC series supports this function.
Product Name
MELSEC-F Series
Product Category
FX3G, FX3U, FX3UC
Series
Main Unit, Engineering Software, GX Works2, GX Developer
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
Communication format setting
Reflecting the changes in the communi...
Operation processing time of the prog...
Communications with a personal comput...
Input numbers of the FX programmable ...
page top
HOME
FAQ