Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
>
Supported versions of the FX3U/FX3UC ...
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
No : 24990
Release Date : 2019/04/23 10:37
Print
Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block
Which versions of the FX3U/FX3UC series main units support the function for accessing the other station of CC-Link using the FX3U-16CCL-M?
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
The main units with Ver.3.10 or later can read and write programs of the FX3 series connected to the intelligent device station and can monitor devices. (GX Works2 with Ver.1.73B or later is applicable.)
Product Name
MELSEC-F Series
Product Category
FX3U, FX3UC
Series
Main Unit, Network/Communication
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
Differences between the FX3UC-32MT-LT...
Connection of the FX3GC series and FX...
Operation of the first special functi...
Supported versions of the FX3G/FX3GC ...
Model of the cable provided with the ...
page top
HOME
FAQ