FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Built-in Ethernet function setting window of MELSEC iQ-R series CPU modules
FAQ
Built-in Ethernet function setting window of MELSEC iQ-R series CPU modules
How can I display the built-in Ethernet function setting window of MELSEC iQ-R series CPU modules?
- Category :
Answer
"Module Parameter" of the CPU module is the setting window.
<Setting a built-in Ethernet port>
[Navigation Window] -> [Parameter] -> [CPU Module] -> [Module Parameter]
<Setting a built-in Ethernet port>
[Navigation Window] -> [Parameter] -> [CPU Module] -> [Module Parameter]
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Security key authentication function of MELSEC iQ-R series
- Combination of the MELSEC iQ-R series inter-module synchronization function and the CC-Link IE Field Network synchronous communication function
- Processing time of when multiple programs are executed with a MELSEC iQ-R series CPU module
- IP filter function of MELSEC iQ-R series CPU modules
- Differences between GX Works3 and GX Works2