FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > How to display the parameter setting window for a programmable controller with GX Works3
FAQ
How to display the parameter setting window for a programmable controller with GX Works3
How can I display the parameter setting window for a programmable controller with GX Works3?
- Category :
Answer
You can display the setting window from a module configuration diagram or system parameters.
<Displaying the setting window from a module configuration diagram>
[Navigation Window] -> [Project] -> [Module Configuration]
<Displaying the setting window from system parameters>
[Navigation Window] -> [Parameter] -> [System Parameter] -> [I/O Assignment]
<Displaying the setting window from a module configuration diagram>
[Navigation Window] -> [Project] -> [Module Configuration]
<Displaying the setting window from system parameters>
[Navigation Window] -> [Parameter] -> [System Parameter] -> [I/O Assignment]
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Overhead time before and after the startup of an interrupt program with a MELSEC iQ-R series CPU module
- Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function
- Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
- Interrupt period setting of fixed scan interrupts of MELSEC iQ-R series
- Processing time of when multiple programs are executed with a MELSEC iQ-R series CPU module