FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Overhead time before and after the startup of an interrupt program with a MELSEC iQ-R series CPU module
FAQ
Overhead time before and after the startup of an interrupt program with a MELSEC iQ-R series CPU module
How long is the overhead time before and after the startup of an interrupt program with a MELSEC iQ-R series CPU module?
- Category :
Answer
Although it depends on interrupt factors, the overhead time before startup becomes 10.8 to 23.8 [us]
and the time after startup becomes 6.5 to 17.4 [us].
and the time after startup becomes 6.5 to 17.4 [us].
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- How to display the parameter setting window for a programmable controller with GX Works3
- GX Developer's compatibility with 64-bit Windows 7
- Relay life of the MELSEC iQ-R series relay output module (RY10R2)
- Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function
- Unable to communicate via USB connection