FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Error code "2401" in QCPU
FAQ
Error code "2401" in QCPU
The error code "2401" has occurred in QCPU.
The Parameter No. under Individual Error Information is "1100H". Are there any remedies?
The Parameter No. under Individual Error Information is "1100H". Are there any remedies?
- Category :
Answer
The error code "2401" is "FILE SET ERROR".
The individual information parameter number "1100H" corresponds to a file register.
The cause of the error is that the file register file specified by the parameter cannot be created.
Check the amount of free space of the memory in which the file register file is created.
The individual information parameter number "1100H" corresponds to a file register.
The cause of the error is that the file register file specified by the parameter cannot be created.
Check the amount of free space of the memory in which the file register file is created.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)