FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Open setting of the built-in Ethernet port QCPU
FAQ
Open setting of the built-in Ethernet port QCPU
When all the 16 ports are configured to use socket communication, is it possible to communicate with GX Developer or GX Works2 through the Ethernet?
- Category :
Answer
No.
It is necessary to configure one port to use the MELSOFT connection.
It is necessary to configure one port to use the MELSOFT connection.
- Product Name
- MELSEC-Q Series
- Series
- CPU