FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > MX Component Version 4's compatibility with 64-bit Windows 7
FAQ
MX Component Version 4's compatibility with 64-bit Windows 7
Does MX Component Version 4 support 64-bit Windows 7?
- Category :
Answer
Yes.
- Product Name
- Engineering Software
- Series
- Middleware
May I have your opinion?
Related FAQ
- Accessing a QnA compatible Ethernet interface module via a router using GX Developer
- Installing MX Component Version 3 and 4
- An error (error code: F1028) occurs when compilation is executed in GX Works2.
- Connection status detection between a hub and the built-in Ethernet port of LCPU
- Automatically assigned devices in GX Works2