Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23419
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:35
  • Print

Using the devices connectable to the GOT1000 series

Answer

The devices connectable to the GOT1000 series can be used with the GOT2000 series as well.
However, some optional devices cannot be purchased due to discontinuation of production. In such a case, please change the equipment configuration or connection type (for example, changing A-bus connection to direct CPU connection).

For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
・ GOT2000 Series Connection Manual (Non-Mitsubishi Electric Products 1) For GT Works3 Version1 (SH-081198ENG)
・ GOT2000 Series Connection Manual (Non-Mitsubishi Electric Products 2) For GT Works3 Version1 (SH-081199ENG)
・ GOT2000 Series Connection Manual (Microcomputers, MODBUS/Fieldbus Products, Peripherals) For GT Works3 Version1 (SH-081200ENG)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication), supported model (controller)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?