FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Compatibility of option units for the GOT1000 series
FAQ
Compatibility of option units for the GOT1000 series
Can the option units for the GOT1000 series be used for the GOT2000 series?
Answer
The following option units for the GOT1000 series can be used for the GOT2000 series as well.
・ GT15-SOUT
・ GT15-PRN
・ GT15-DIOR
・ GT15-DIO
The following option units for the GOT1000 series cannot be used.
Please replace them with the option units dedicated to the GOT2000 series (GT27***).
・ GT16M-MMR → GT27-MMR-Z
・ GT16M-V4 → GT27-V4-Z
・ GT15V-75V4 → GT27-V4-Z
・ GT16M-R2 → GT27-R2, GT27-R2-Z (*)
・ GT15V-75R1 → GT27-R2, GT27-R2-Z (*)
・ GT16M-V4R1 → GT27-V4R1-Z
・ GT15V-75V4R1 → GT27-V4R1-Z
・ GT16M-ROUT → GT27-ROUT, GT27-ROUT-Z
・ GT15V-75ROUT → GT27-ROUT, GT27-ROUT-Z
(*) The settings for GT27-R2 and GT27-R2-Z differ in the screen design software.
The following option units for the GOT1000 series cannot be used.
Please change the equipment configuration such as adding a USB memory.
・ GT15-CFCD
・ GT15-CFEX-C08SET
・ GT15-SOUT
・ GT15-PRN
・ GT15-DIOR
・ GT15-DIO
The following option units for the GOT1000 series cannot be used.
Please replace them with the option units dedicated to the GOT2000 series (GT27***).
・ GT16M-MMR → GT27-MMR-Z
・ GT16M-V4 → GT27-V4-Z
・ GT15V-75V4 → GT27-V4-Z
・ GT16M-R2 → GT27-R2, GT27-R2-Z (*)
・ GT15V-75R1 → GT27-R2, GT27-R2-Z (*)
・ GT16M-V4R1 → GT27-V4R1-Z
・ GT15V-75V4R1 → GT27-V4R1-Z
・ GT16M-ROUT → GT27-ROUT, GT27-ROUT-Z
・ GT15V-75ROUT → GT27-ROUT, GT27-ROUT-Z
(*) The settings for GT27-R2 and GT27-R2-Z differ in the screen design software.
The following option units for the GOT1000 series cannot be used.
Please change the equipment configuration such as adding a USB memory.
・ GT15-CFCD
・ GT15-CFEX-C08SET
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Option unit
- Series
- GOT2000 Series