FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Compatibility of the option board for the MES interface function
FAQ
Compatibility of the option board for the MES interface function
Can the option board for the MES interface function for the GOT1000 series be used for the GOT2000 series?
Answer
The option board for the MES interface function for the GOT1000 series (GT16-MESB/GT15-MESB48M) cannot be used for the GOT2000 series.
Use the license of the MES interface function for the GOT2000 series (GT25-MESIFKEY).
In addition, when the BootOS version of the GOT is "C" or earlier, updating the BootOS version to "D" or later is required.
* To update the BootOS version to "D" or later, GT Designer3 (GOT2000) Version1.108N or later is required.
For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
"4.3.2 Transferring data" or
"4.5.3 Installing the BootOS or the CoreOS to the GOT"
Use the license of the MES interface function for the GOT2000 series (GT25-MESIFKEY).
In addition, when the BootOS version of the GOT is "C" or earlier, updating the BootOS version to "D" or later is required.
* To update the BootOS version to "D" or later, GT Designer3 (GOT2000) Version1.108N or later is required.
For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
"4.3.2 Transferring data" or
"4.5.3 Installing the BootOS or the CoreOS to the GOT"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Option (option function board), GOT function (MES interface)
- Series
- GOT2000 Series