Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23437
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:51
  • Print

Compatibility of the wireless LAN communication unit (GT25-WLAN)

Can the wireless LAN communication unit be used with the GT27 model that had been purchased before the wireless LAN communication unit (GT25-WLAN) was released?
Category : 

Answer

The wireless LAN communication unit (GT25-WLAN) can be used when the BootOS version of the GOT is "C" or later. When the BootOS version of the GOT is "B" or earlier, the wireless LAN communication unit (GT25-WLAN) is not recognized. Please update the BootOS.

* To update the BootOS version to "C" or later, GT Designer3 (GOT2000) Version1.105K or later is required.

For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
 "4.3 Transferring the Data between the Personal Computer and the GOT" or
 "4.5.3 Installing the BootOS or the CoreOS to the GOT"

* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
 ・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Communication unit
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?