FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 > Compatibility of the wireless LAN communication unit (GT25-WLAN)
FAQ
Compatibility of the wireless LAN communication unit (GT25-WLAN)
Can the wireless LAN communication unit be used with the GT27 model that had been purchased before the wireless LAN communication unit (GT25-WLAN) was released?
Answer
The wireless LAN communication unit (GT25-WLAN) can be used when the BootOS version of the GOT is "C" or later. When the BootOS version of the GOT is "B" or earlier, the wireless LAN communication unit (GT25-WLAN) is not recognized. Please update the BootOS.
* To update the BootOS version to "C" or later, GT Designer3 (GOT2000) Version1.105K or later is required.
For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
"4.3 Transferring the Data between the Personal Computer and the GOT" or
"4.5.3 Installing the BootOS or the CoreOS to the GOT"
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
* To update the BootOS version to "C" or later, GT Designer3 (GOT2000) Version1.105K or later is required.
For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
"4.3 Transferring the Data between the Personal Computer and the GOT" or
"4.5.3 Installing the BootOS or the CoreOS to the GOT"
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Communication unit
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Wireless LAN communication unit and wireless LAN access point
- Remote personal computer operation function (Ethernet)
- Using with the GOT1000 series in the client/server function
- Changing the bus connection to the Ethernet connection
- Connecting FA devices through the wireless LAN communication unit (GT25-WLAN)