Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23443
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:59
  • Print

Ethernet connection between multiple GOTs and the QnUDVCPU

I want to connect multiple GOT2000 series models and one QnUDVCPU by Ethernet by using the Ethernet port built in the CPU.
How can I set it?
Category : 

Answer

The following describes an example of settings to connect multiple GT27, GT25, or GT21 models (Ethernet connection models) and the Ethernet port built in the QnUDVCPU by Ethernet.

1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
 (1) Select [Common] → [Controller Setting] → [CH1] from the menu.
   Manufacturer: MITSUBISHI ELECTRIC
   Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
   I/F: Ethernet:Multi
   (For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
   Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
   (For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
   GOT Net No.: 1
   GOT Station: 18
 (2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
   Host: *
   Net No.: 1 (example)
   Station: 1 (example)
   Unit Type: QnUD(P)V/QnUDEH
   IP address 192.168.3.39
   Port No. 5006
   Communication: UDP
 (3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
 (For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting] from the menu.)
   GOT IP address: 192.168.3.18
   Subnet Mask: 255.255.255.0
 (4) Set a different station number and GOT IP address for (1) to (3) above for each GOT.

2. Configure the following settings in GX Works2.
 (1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
   IP address: 192.168.3.39
   Subnet Mask Pattern: 255.255.255.0
 (2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
   Protocol: UDP
   Open System: MELSOFT Connection (Set this item for each GOT.)

For the details, refer to the following.

・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
 "5.3 GOT Side Settings"
 "5.4 PLC Side Setting"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries