Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23448
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 17:09
  • Print

Use of the Ethernet cable

Which Ethernet cable can be used for the Ethernet connection between a GOT2000 series model and a Mitsubishi Electric PLC, a cross cable or straight cable?
Category : 

Answer

The Ethernet cable that can be used for the Ethernet connection between a GT27, GT25, or GT21 model (Ethernet connection models) and a Mitsubishi Electric PLC differs depending on the controller and with/without a hub.
Please use the following cables according to configuration of the connection.

1. For connecting the GOT and the PLC via a hub
 Straight cable
 (When the hub supports AutoMDI/MDI-X, both a straight cable and cross cable can be used since the hub has the automatic identification function for the port.)

2. For connecting the GOT and the PLC without a hub
 (1) For connecting the GOT to the Ethernet module of the PLC
   Cross cable
 (2) For connecting the GOT to the Ethernet port built in the PLC
   Straight cable or cross cable
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Cable
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?