FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Use of the Ethernet cable
FAQ
Use of the Ethernet cable
Which Ethernet cable can be used for the Ethernet connection between a GOT2000 series model and a Mitsubishi Electric PLC, a cross cable or straight cable?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
The Ethernet cable that can be used for the Ethernet connection between a GT27, GT25, or GT21 model (Ethernet connection models) and a Mitsubishi Electric PLC differs depending on the controller and with/without a hub.
Please use the following cables according to configuration of the connection.
1. For connecting the GOT and the PLC via a hub
Straight cable
(When the hub supports AutoMDI/MDI-X, both a straight cable and cross cable can be used since the hub has the automatic identification function for the port.)
2. For connecting the GOT and the PLC without a hub
(1) For connecting the GOT to the Ethernet module of the PLC
Cross cable
(2) For connecting the GOT to the Ethernet port built in the PLC
Straight cable or cross cable
Please use the following cables according to configuration of the connection.
1. For connecting the GOT and the PLC via a hub
Straight cable
(When the hub supports AutoMDI/MDI-X, both a straight cable and cross cable can be used since the hub has the automatic identification function for the port.)
2. For connecting the GOT and the PLC without a hub
(1) For connecting the GOT to the Ethernet module of the PLC
Cross cable
(2) For connecting the GOT to the Ethernet port built in the PLC
Straight cable or cross cable
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Cable
- Series
- GOT2000 Series