Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23450
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 17:12
  • Print

Changing the bus connection to the Ethernet connection

I want to change the connection type between the GOT2000 series model and Q06HCPU from the one-on-one Q-bus connection to the Ethernet connection.
Which settings for the GOT are required to be changed?
Category : 

Answer

To change the connection type between the GT27 or GT25 model and the Q06HCPU from the one-on-one Q-bus connection to the Ethernet connection, change the following settings in the controller setting on GT Designer3 (GOT2000).

1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
 (1) Select [Common] → [Controller Setting] → [CH1] from the menu.
  ・ I/F setting
    Extend I/F(1st) → Ethernet:Multi
   (For GT Designer3 (GOT2000) Version1.170C or later, Standard I/F(Ethernet): Multi)
  ・ Driver setting
    Bus(Q) → Ethernet(MITSUBISHI ELECTRIC), Gateway
   (For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
 (2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
  Default values are set. Please change the settings according to the configuration of the connection.
 (3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
 (For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting] from the menu.)
  Please change the settings according to the configuration of the connection.

2. Configure the following settings in GX Works2.
 Please configure the settings of the built-in Ethernet port or network parameter according to the configuration of the connection.

For the details, refer to the following.

・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
 "5.3 GOT Side Settings"
 "5.4 PLC Side Setting"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?