Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23452
  • Release Date : 2018/09/14 15:06
  • Print

Screen gesture mode and overlap window display

While an overlap window is displayed, if the mode is switched to the screen gesture mode, how is the overlap window displayed?
Category : 

Answer

While an overlap window is displayed, if the mode is switched to the screen gesture mode, the overlap window is hidden.
The overlap window is redisplayed when the screen gesture mode is disabled.

Note that in the screen gesture mode, the screen switching device of the overlap window retains the screen number of the overlap window displayed before the mode was switched to screen gesture mode.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (standard function)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?